Date Picker | Web Component

The default date format for the <dk-date-picker /> is "MM/dd/yyyy". To change the format add a format prop on the date picker and set a string format based on this spec.

"MM/dd/yyyy": "yyyy/MM/dd":

Properties

Use properties and attributes to control the web component as well as pass required data to it. Some properties won't have an attribute name, this is because to use that property you can't use it as an html attribute it must be set using javascript as a property of the element.

PropertyAttributeDescriptionTypeDefault
formatformatPass a string that follows the unicode token spec: Unicode Specstring"MM/dd/yyyy"
labellabelUse this to set the label of the date picker.stringnull
maxDateStringmaxSet's the max date that can be selected. Must match the date format set on the component. The default is "MM/dd/yyyy"stringnull
minDateStringminSet's the min date that can be selected. Must match the date format set on the component. The default is "MM/dd/yyyy"stringnull
openopenSet this property to true or false to control if the picker is open or notbooleanfalse
rangerangeEnables date range selectionbooleanfalse
typedRangeundefinedWhen using a range date picker an object that store the selected values will be store here.{ start: Date; end: Date; }{start: null, end: null}
typedValueundefinedThis property holds the value of the current selected date. It is a JS Date Object.Datenull
valuevalueThe date string for the selected date. It must be in the "MM/DD/YYYY" format.stringnull
valueEndvalue-endThe date string of the end of the selected range.stringnull
valueStartvalue-startThe date string of the start of the selected range.stringnull

Events

EventDescriptionType
dkChangeThe change event is fired whenever a user has picked a date. If it is a range picker the selected property will be an object with the start and end.{ selectionType?: SelectionType; selected: Date

Format

<dk-date-picker format="yyyy/MM/dd"></dk-date-picker>

Label

<dk-date-picker
        label="Labeled date picker"
        min="01/01/2020"
        max="12/29/2020"></dk-date-picker>

Preset

<dk-date-picker
        value="03/04/2020"
        min="01/01/2020"
        max="12/29/2020"></dk-date-picker>

Range

<dk-date-picker range="true"></dk-date-picker>

Range Preset

<dk-date-picker
        range="true"
        value-start="03/03/2020"
        value-end="04/01/2020"></dk-date-picker>

Single

<dk-date-picker></dk-date-picker>