Add the classname dk-card to any wrapper element to add the card styles of background-color, border, border-radius and box-shadow. Cards by default do not have any padding or margin and will need that added as needed.
Code Example:
<div class="dk-card">
Default card with no padding or margin.
</div>
<div class="dk-card p-2 my-2">
Card with padding and margin (p-2 adds 16px padding to all sides).
</div>
<div class="dk-card--blue p-2">
Blue card option using `dk-card--blue` class name and padding (p-2 adds 16px padding to all sides).
</div>
Code Preview:
Interactive Card
If you have a card that requires interactive hover styles use the classname dk-card--interactive.
Code Example:
<div class="dk-card--interactive p-2">
Interactive card showing hover effects.
</div>
Code Preview:
Cards in Cards
When a card is placed inside another card the box shadow gets set to a border.
Code Example:
<div class="dk-card p-3">
<div class="test-box">
Card A
<div class="dk-card p-3 my-2">
Card B
<div class="dk-card--interactive p-3 my-3">
Card C: The final Card
</div>
</div>
</div>
</div>Code Preview:
Marketing Cards
This is an example of a marketing card with an image.
Code Example:
<div class="dk-card dk-card--marketing">
<div class="dk-card--marketing__img">
<img src="https://bit.ly/2TRyrfw" alt="Image Alt Text" />
</div>
<div class="dk-card--marketing__content">
<h1 class="dk-card--marketing__title">
With Button
</h1>
<p class="dk-card--marketing__snippet">
A long but limited description
that gives the user context about
what product, service, or area
they are clicking into, but not
too much information as to
overload them.
</p>
<button class="dk-btn__primary">
Button Text
</button>
</div>
</div>